Hi,
I'm using a single LTM2881HV-3 on a 6-layer board for isolated RS-485. During radiated emissions testing (CISPR 32 Class A, 30 MHz - 1 GHz), we're seeing a strong 4 MHz fundamental with harmonics extending up to 125 MHz. Several harmonics in the 60-100 MHz range exceed the QP limit. Using near-field probes, we confirmed the source is the LTM2881's internal DC-DC.
Here is the layout around U29 and the test results from the lab:

What we've tried:
- Low EMI mode enabled
- Low ESL decoupling caps on VCC and VISO
- Ferrite beads on the RS-485 A/B bus lines
- Tying all mounting holes to the earth guard ring
- Ground braid between chassis and earth (reduced low-frequency content but 60-100 MHz range still fails)
A few things I'm not sure about:
-
Stitching capacitor placement. We currently have a discrete capacitor between GNDISO and the earth guard ring, but not a direct stitching cap between GND and GNDISO. Our 6-layer stackup makes it difficult to overlap GND and GNDISO planes for an embedded stitching capacitor. Should I be prioritizing a discrete cap directly between GND and GNDISO as close to U29 as possible instead? Would that be more effective for the 60–100 MHz range than our current GNDISO-to-earth connection?
-
Ferrite keep-out. We have ferrites on the A/B lines but I'm not confident about the copper keep-out underneath. Should all copper be removed under the ferrite pads, or just the isolated-side ground pour? Do I also need ferrites on the VISO and GNDISO lines leaving the "hot" area?
-
For the next revision we are considering the ADM2561E as a replacement. Is the DC-DC in that part fundamentally lower-emission than the LTM2881's, or would we face similar layout challenges?
Thanks,
Jordi
Edit Notes
updated images[edited by: jordicook at 3:57 PM (GMT -4) on 18 Jun 2026]