Post Go back to editing

Load current capability of ADUM360N

Thread Summary

The user inquires about the Iox capability of the ADUM360N when operating at 5V. The final answer confirms that the ADUM360N can handle a continuous load of up to 4mA at 5V, with an average of +/-10mA as per the Abs Max table. It is suggested to consider adding a relay driver or similar component for continuous DC loads.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADUM360

HI 

I'm planning to use ADUM360N in my design. then I would like to know Iox capability of ADUM360N.

According to P7 of the datasheet, I could confirm Iox test condition and it could use by 4mA load when it operates 5V.

However, I would like to know this spec as ADUM360N.

Best regards

Parents Reply Children
No Data