Post Go back to editing

VDDB pin current of MAX22025AWA+

Thread Summary

The user inquires about the VDDB pin current consumption of the MAX22025AWA+ during communication. The final answer explains that the IDDB current is the sum of the internal current (4.0 to 5.5mA when TxD is low) and the output current, which depends on the load and bus configuration. The transmitter output characteristic plots on page 15 can help estimate the driver's Thevenin resistance for specific load conditions.
AI Generated Content
Category: Datasheet/Specs

Hello, 

Thank you for your always our support.
Regarding VDDB pin current of MAX22025AWA+ during communication, I would like to confirm.
When there is no communication, in the datasheet that the Supply Current IDDB = 4.0 to 5.5mA on page 7, but how is the current consumption during communication?

Does the MAX22025AWA+ consume approximately 20-30mA ,or more during serial communication (It depends on the load connection situation...)?


Thank you.
Best regards,



 


Edit Notes

Comment correction
[編集者:S1640、編集時刻: 7 Jan 2026 日 5:25 AM 時 (GMT -5)]
Parents
  • As you correctly mention, the total current flowing into VDDB, IDDB, depends on the external load conditions.

    The IDDB current will be a combination of the current consumed internally by the transceiver which will depend on the state of the transceiver and the output current driving the load which depends on the output driver state and the external load / bus.

    The EC table lists the IDDB when TxD is low which is the higher current operational state - this can be inferred from the supply current vs temperature plots on page 14 which show plots with TxD low and high.  The low plots all have slightly higher currents than the high plots and so are a reasonable choice for the part's internal current consumption.

    The MAX22025's drivers are only active under specific conditions, see the Function tables on pg 17.  The transmitter output characteristic plots on page 15 can be used to estimate the driver's Thevenin resistance which then can be used in the computation of the output current for the particular load/bus configuration.

    The IDDB current is then the sum of the internal current plus the output current into the bus.

    Eric

Reply
  • As you correctly mention, the total current flowing into VDDB, IDDB, depends on the external load conditions.

    The IDDB current will be a combination of the current consumed internally by the transceiver which will depend on the state of the transceiver and the output current driving the load which depends on the output driver state and the external load / bus.

    The EC table lists the IDDB when TxD is low which is the higher current operational state - this can be inferred from the supply current vs temperature plots on page 14 which show plots with TxD low and high.  The low plots all have slightly higher currents than the high plots and so are a reasonable choice for the part's internal current consumption.

    The MAX22025's drivers are only active under specific conditions, see the Function tables on pg 17.  The transmitter output characteristic plots on page 15 can be used to estimate the driver's Thevenin resistance which then can be used in the computation of the output current for the particular load/bus configuration.

    The IDDB current is then the sum of the internal current plus the output current into the bus.

    Eric

Children
No Data