I do not plan on using the LPCM feature with the ADBMS6822 and is wondering what I should do with the INTR and RTO pins?
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Missed after 706 hours |
WHong |
Open |
ADBMS6822
Production
The ADBMS6821 (single) and ADBMS6822 (dual) provide bidirectional isolated serial port interface (isoSPIâ„¢) communications between two isolated devices...
Datasheet
ADBMS6822 on Analog.com
I do not plan on using the LPCM feature with the ADBMS6822 and is wondering what I should do with the INTR and RTO pins?
You can leave them floating if you are not using INTR and RTO pins.
You can leave them floating if you are not using INTR and RTO pins.