I do not plan on using the LPCM feature with the ADBMS6822 and is wondering what I should do with the INTR and RTO pins?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADBMS6822
Production
The ADBMS6821 (single) and ADBMS6822 (dual) provide bidirectional isolated serial port interface (isoSPIâ„¢) communications between two isolated devices...
Datasheet
ADBMS6822 on Analog.com
I do not plan on using the LPCM feature with the ADBMS6822 and is wondering what I should do with the INTR and RTO pins?
You can leave them floating if you are not using INTR and RTO pins.