Post Go back to editing

The camera extension line designed with MAX96717 has image flickering issues

Category: Hardware
Product Number: MAX96717
      The camera designed with MAX96717 works normally in 3Gbps mode, but when connected to a certain distance extension cable (such as 10 meters) at 6Gbps, there may be image flickering issues, which occur every once in a while.The schematic diagram was designed based on the manual. Is it due to PCB layout? For example, is the adjacent layer of the POC link the signal layer instead of the GND layer, or is the POC link layer covered with ground copper?
      In addition, the volume of the inductor used in the specification sheet is too large for my design. Do you have any other recommended inductor models?
      The hope can obtain your reply, thanks!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.