Post Go back to editing

Can GND be used as reference voltage

Category: Hardware
Product Number: ADUM4195

Hello ADI team,

I am planning to use isolated amplifier to remove 50 Hz ground loop from my application. I have decided to use ADUM4195 amplifier. However my concern is with reference voltage. My signal is singled ended signal centered around 0V, can I give 0V as reference to ADUM4195 non inverting pin instead of reference voltage output provided by amplifier. I will be using it also for calibration purpose of my sensor, my requirement is that signal should be centered around the 0V for proper calibration. Having DC offset of 1.25 or 2.5V is extremely undesirable.

Second question, will the use of isolation amplifier eliminate the 50 Hz ground loop I am observing?

Please answer my question at earliest, as this design is time sensitive project.

  • Hi  

    Thanks for the question.

    The connection to VREF (marked with a red dot in the image below) is intended to provide a positive DC bias to the input signal. This ensures that the signal remains within the amplifier’s valid input voltage range, which is between 0.25 V and VDD2 – 0.7 V.

    If the input signal is centered around 0 V, it would include negative voltage components that fall outside the amplifier’s operating range. As a result, the output (VOUT) would be distorted or clipped during those portions of the waveform, effectively making the amplifier "blind" to the negative part of the signal.

    For what concern the calibration on your application, is your sensor calibrated with the input voltage or with the output voltage?

    Regards,
    Alessandro