Hi tech support,
I am using ADuM3220 as a floating gate driver to drive a pair of MOSFETs that had both source pins tied together, and both gate pins tied together, as a solid state relay. This configuration is used in order to keep the MOSFET body diode from conducting when Vgs is off. Everything works fine except I noticed that the output (to gates of the MOSFET pair) swings from zero to 20 volts, while the isolated supply itself is only 14 volts. why and how is the output boosted to 20V? I'm not aware of such boost descriptions in the datasheet.
The external floating supply + is connected to pin-8 and supply ground is connected to pin-5.
Thanks for your help,
Larry