Post Go back to editing

Operating output Voltage

Category: Hardware
Product Number: ADuM3123

Hello!

I want to use ADUM3123 as a negative supply voltage switch. I will supply -5V to pin 5 and (-2.7..-2.2V) to pin 8. Will ADUM switch between these two voltages?

Parents Reply
  • The Hysteresis by definition is the difference between Positive going threshold and Negative going threshold.
    So, the difference between VDD2 and GND2 should be > 3.6V to not trip the UVLO protection on Grade A devices.
    If you trip the UVLO protection, you need additional 0.5V to exit the UVLO error condition. 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.