Hello!
I want to use ADUM3123 as a negative supply voltage switch. I will supply -5V to pin 5 and (-2.7..-2.2V) to pin 8. Will ADUM switch between these two voltages?
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADuM3123
Production
The ADuM3123 is a 4.0 A isolated, single channel driver that employs Analog Devices, Inc. iCoupler® technology to provide precision isolation. The ADuM3123...
Datasheet
ADuM3123 on Analog.com

Hello!
I want to use ADUM3123 as a negative supply voltage switch. I will supply -5V to pin 5 and (-2.7..-2.2V) to pin 8. Will ADUM switch between these two voltages?
Please refer to the Undervoltage Lockout (UVLO) section on the datasheet for VDD2.
In this section is specified the minimum voltage required between VDD2 and GND2 for the part to operate.
Regards,
Luca

The date is not written clearly. How do you understand this table? The difference between VDD2 and GND2 should be 3.2V or 0.5VThe Hysteresis by definition is the difference between Positive going threshold and Negative going threshold.
So, the difference between VDD2 and GND2 should be > 3.6V to not trip the UVLO protection on Grade A devices.
If you trip the UVLO protection, you need additional 0.5V to exit the UVLO error condition.