Post Go back to editing

ADUM4121WHB1Z shoot through

Thread Summary

The user is experiencing a low voltage square wave on the negative side of the drive output with the ADUM4121WHB1Z evaluation board, which may indicate shoot through. The support engineer suggests checking for ground loops and using isolated or differential probes to measure the high-side gate voltage. The user provided scope captures showing noise on other channels when the daughter board is installed, and the issue worsens with high voltage. The support engineer requested a scope capture without the power daughter cards to further diagnose the problem.
AI Generated Content
Category: Hardware
Product Number: adum4121WHB1Z, adum4121

I am currently using the ADUM4121WHB1Z evaluation board with the Wolfspeed system. Without the daughter boards installed for the mosfets, I see a low voltage squarewave on the negative side of the drive output. It looks like when I try drive the half bridge, it is creating shoot through. I had to replace the drivers a couple times over a shoot through event. Is there anything else I should be looking at?

Parents
  • Hi JimmyH,

    Thanks for getting in touch regarding the ADUM4121WHB1Z

    To better understand the issue could you please provide more information on what net of the circuit are you probing, and provide a scope capture of the waveform showing the square wave?
    What Wolfspeed system are you using, and how are you driving the PWM signals on connector P2?

    Thanks,
    Luca
      


  • Hi Luca,

    Yes, I am using the SpeedVal kit Three-phase motherboard. Yes I am connecting to it as normal. I am not using the processor daughter card, but connecting single ended pwm to the PWM monitor conn11. I have made no modifications to the ADUM4121WHB1Z, but I have had to replace the drivers a couple times. We are running at 6khz with a deadtime of 10uS. We are using to create a full bridge rectifier if that helps. Channel one is the output of the Driver. One picture for low side and one for High side.

     

    Thanks,

    Jimmy

  • Hi Jimmy,

    I think you might have some setup issue here, such as ground loop through GND of scope probes or something else, I don't believe this ripple is coming from the gate driver.
    Are you using isolated probes or differential probes to measure high side gate voltage?   
    Can you take the same scope capture without the power daughter cards please?
    I would like to see the output of the gate driver when the power transistor is removed.

    Thanks,
    Luca

  • Luca, 

    Thanks for responding. I was pulled to other things. Below I have taken better screen shots. One is with no Daughter board installed and the other is with the daughter board installed but without High voltage. If I turn on any high voltage, it gets worse.

    No daughter card  Daughter card installed, no high voltage

    In the first image you can see that the Rise and fall are creating noise on the other 3 channels. This is the output of the driver board. In the second image, you can see this noise gets worse if I install the daughter board. With out these, there is no noise. I did have a shoot through that damaged a couple driver boards and I have replaced the ADUM4121 for both boards and High and Low side. If there was something else I should replace it would be greatly appreciated.

    Thanks,

    Jimmy

Reply
  • Luca, 

    Thanks for responding. I was pulled to other things. Below I have taken better screen shots. One is with no Daughter board installed and the other is with the daughter board installed but without High voltage. If I turn on any high voltage, it gets worse.

    No daughter card  Daughter card installed, no high voltage

    In the first image you can see that the Rise and fall are creating noise on the other 3 channels. This is the output of the driver board. In the second image, you can see this noise gets worse if I install the daughter board. With out these, there is no noise. I did have a shoot through that damaged a couple driver boards and I have replaced the ADUM4121 for both boards and High and Low side. If there was something else I should replace it would be greatly appreciated.

    Thanks,

    Jimmy

Children
No Data