Post Go back to editing

Question about moisture detection when using PD Cable of MAX20342

Category: Datasheet/Specs
Product Number: MAX20342
I uses MAX20342 to detect moisture in USB Type C Connector.

If I connect only Type C PD Cable to this MAX20342's Type C connector without PD source like adapter, the resistance value measured at CC is 1.103KOhm, so it is detected as if there is moisture even though there is no moisture.

How can I solve this?

Edit Notes

L-Maxim product
[edited by: AAlessandro at 9:26 AM (GMT -4) on 4 Jun 2025]