Post Go back to editing

MAX3421E Lifecycle

Category: Hardware
Product Number: MAX3421E

The MAX3421E SPI USB Peripheral/Host Controller comes in two packages:

MAX3421EEHJ+ = TQFP-32

MAX3421EETJ+ = TQFN-32

The MAX3421EEHJ+ TQFP-32 package is now listed on Product Discontinuation Notices: https://www.analog.com/media/en/PCN/m001117.pdf 

But there is no mention of the MAX3421EETJ+ TQFN-32 package being discontinued.  Is there someone at Analog that can update the lifecycle information for the MAX3421EETJ+?

This is a convenient part because it has a SPI interface, can be used as either a USB Host or Peripheral, and has drivers integrated into standard Linux.  I'm hoping to hear that Analog will manufacture this for years to come.

Edit Notes

tag added. L-Maxim product
[edited by: AAlessandro at 10:02 AM (GMT -4) on 26 May 2025]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.