In the block diagram below, I’m using an isolated RS422(ADM2390EBRWZ) transceiver. My system includes the diodes shown in the diagram, but there is no GDT between the two isolated grounds. During ESD testing with an ESD gun, the TVS diodes were ineffective, and my system suffered significant damage. (Note: the ESD gun's reference is connected to system "GND", and the ESD pulses are applied to the RS422 pins.)
My question is: where should I connect the reference ground of the ESD gun during testing? Should it be tied to chassis ground, to the isolated ground ("GND_ISO"), or to the system ground ("GND")?
Additionally, if I connect the ESD gun’s reference to either the chassis or the system ground, would it be reasonable to place a GDT between the isolated ground and the system/chassis ground as shown in the block diagram?