Post Go back to editing

Gate driver requirement for SiC MOSFET from microchip MSC025SMA330B4N

Thread Summary

The user is seeking a gate driver for a 3300V SiC MOSFET with a total gate charge of 410 nc and a fall time of 26 ns, requiring a minimum gate driver current of 16-17A and a minimum withstand isolation voltage of 5000V. The final answer asks about the creepage requirement and whether PCB potting or conformal coating is an option for the gate driver PCB.
AI Generated Content
Category: Hardware
Product Number: ADuM4177

Hi ADI community

I am working on SST project. In this project we are Planning to use 3300V SiC MOSFET from the microchip. For this MOSFET has the Total gate charge has 410 (nc) and fall time is 26(ns) total gate drive current requirement is 410/26 which is more than 16A

So please suggest the gate driver from Analog Devices which can support Working voltage is more than 2800V.

Minimum withstand isolation voltage is more than 5000V.

Minimum gate driver current should be 16 or 17A.

and It should contain the DESAT features.

I am inserting example technical specification i required please go through that suggest  some gate drivers according to my requirement

If any other gate driver suggestion any other manufactures suggest me also