KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADM3315E
Production
Operating from a single supply as low as +2.7 V, the ADM3315E is a three-driver/three-receiver serial port transceiver, and fully meets full EIA-232 standards...
Datasheet
ADM3315E on Analog.com
Hello,
Thank you for your inquiry. I would be happy to help you.
The maximum rating for the RIN pins on both the ADM3315E and ADM101E is +/-30V. Unfortunately, I was not able to find any isolated RS-232 transceivers with RIN ratings greater than +/-30V. We have only one device that meets your voltage withstand requirements and that is the MAX13223E.
For RS-485: only one isolated transceiver features a maximum rating above +/-32V for the bus IOs, and that is the ADM2795E. Please take a look and verify if this device meets your other needs (e.g. supply voltage, data rate, isolation rating). We have a number of non-isolated RS-485 transceivers with maximum ratings above +/-30V, but they would need to be used with an isolator, if isolation is needed.
Thank you,
Shasta