Post Go back to editing

Looking for a Replacement SerDes pair with MIPI to GMSL and GMSL to Parallel Data output

Thread Summary

The user inquired about using a CSI-2 serializer (e.g., MAX96751) with the MAX9276A deserializer to convert a CSI-2 signal to a parallel output. The final answer directed the user to Analog Devices' technical support pages for further assistance, as no direct solution was provided. Relevant products: MAX9275, MAX9276A, MAX96751.
AI Generated Content
Category: Hardware
Product Number: MAX9275

Right now I am using the MAX9275 - MAX9276A SerDes pair, which has Parallel to GMSL to Parallel configuration.

Currently, I am looking to develop a SerDes system with the configuration of CSI-2 to GMSL to Parallel.
I looked through all the available devices, but I didn't find any that matched this configuration.

My query is, suppose I use any CSI-2 Serialiser (ex MAX96751). Can I use MAX9276A to deserialise the GMSL signal to Parallel output? 
Will this work??

Edit Notes

Lagacy Maxim product
[edited by: AAlessandro at 1:22 PM (GMT -4) on 17 Mar 2025]