Post Go back to editing

ADUM4177 VDD1 ramp rate requirement

Category: Datasheet/Specs
Product Number: ADUM4177

Hi,
In the datasheet, on Page 17 under the "VDD1 Supply" section, it states, "The ramp rate on the VDD1 pin must be kept below 1 V/ms." However, in Figure 5, the ramp rate of VDD1 appears to be much faster than this.
Is the limitation of dv/dt rate < 1 V/ms  correct, or is dv/dt rate > 1 V/ms required?

  • Hi Jeams13,

    Please let me verify the ramp rate spec with the design team and I'll get back to you. 

    Thanks,
    Luca

  • I have obtained an answer from the design team to your question on the supply ramp requirements of ADuM4177.
    The datasheet sentence:
    “The ramp rate on the VDD1 pin must be kept below 1 V/ms to avoid stress on the primary side silicon. Both startup and operation have this dv/dt rate limitation.”


    Is NOT valid for the released silicon, this was a limitation of early silicon, fixed at later stage.
    Unfortunately, this sentence has not been removed from the released datasheet. We’ll fix this typo in the next datasheet revision.

    I can confirm that:

    • The ADuM4177 is safe to operate with a 4.4V – 7V VDD1 supply and a power supply ramp rate that matches the 5us ramp shown in the IC1 power up delay test.
    • The safe range of power-up ramp for ALL supply rails is conservatively ~2us.
    • For power up ramps in the 50ns to 2us range, contact ADI.
    • After power up, supply jumps of up to 1V should be limited to 2us rise-time/fall-time and longer.

       
    Thanks,
    Luca

  • Thank you for your confirmation and clarification. I understand the ramp rate limitation on the VDD1.

    Best Regards,