Post Go back to editing

VDD2 = 5.5 V when power on

Category: Hardware
Product Number: ADUM4165

Hi there, 

I am working on a USB isolator based on the ADUM4165. However, when I apply 5.5V to VBUS2, VDD2 is not behaving as expected. Instead of outputting 3.3V, it is showing 5.5V, which is equal to the VBUS2 voltage.

Any suggestions will be appreciated.

Thanks in advance.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.