ADUM4165
Recommended for New Designs
The ADuM4165/ADuM41661 are USB 2.0 port isolators, utilizing Analog Devices, Inc., iCoupler® technology to dynamically support all USB 2.0 data rates;...
Datasheet
ADUM4165 on Analog.com
Hi there,
I am working on a USB isolator based on the ADUM4165. However, when I apply 5.5V to VBUS2, VDD2 is not behaving as expected. Instead of outputting 3.3V, it is showing 5.5V, which is equal to the VBUS2 voltage.
Any suggestions will be appreciated.
Thanks in advance.
Hello,
Can you please provide details on how you are providing the clock to ADuM4165?. If possible, can you share circuit schematics with us to debug the issue better (here or via Email: prasanthi.yerra@analog.com)
Hello, here is the schematic

Hello, any idea of it?