Post Go back to editing

What are voltage threshold in HTL mode (current source off)?

Category: Datasheet/Specs
Product Number: MAX22196

Hi

For MAX22196, if CNFGx register is configured with CURRx[1:0]=00 (current source off) , what are voltage threshold on input? I don't find its in datasheet. Table 1 shows that HIHTR don't care. Are they different if CURRx[1:0]=11.

In my application, REGEN is short to ground, V24=24V, VA=3.3V and REFDI=12k.

Thanks for your help.

Parents
  • Hello,

    My apologies for the delayed response on this.  

    I can see how the don't care (X) label is a bit misleading in this case.  While the status of the HITHR bit is not required to set the mode to high-impedance or HTL (CURR_ = 00) , it is still required to set the thresholds, as outlined in the datasheet. You need to set the SOURCE and HITHR bits for a given channel to set the threshold, as shown in the EC table on pages 5-6.

    Setting the CURR_ bits to 11 will put the input channel into TTL mode.  The TTL thresholds are also shown in the EC table.

    Thank you,

    Shasta

Reply
  • Hello,

    My apologies for the delayed response on this.  

    I can see how the don't care (X) label is a bit misleading in this case.  While the status of the HITHR bit is not required to set the mode to high-impedance or HTL (CURR_ = 00) , it is still required to set the thresholds, as outlined in the datasheet. You need to set the SOURCE and HITHR bits for a given channel to set the threshold, as shown in the EC table on pages 5-6.

    Setting the CURR_ bits to 11 will put the input channel into TTL mode.  The TTL thresholds are also shown in the EC table.

    Thank you,

    Shasta

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.