Hi Team,
We are planning to use LTC4312 IC to switch a I2C slave device between two masters similar to the application diagram shown in the datasheet

In the application circuit with dual master configuration, the power pin VCC2 is grounded
Please let me know when we make VCC2 Power pin to ground, the I2COUT1 and I2COUT2 will work. As per the application circuit it shows like the VCC2 powers the OUT Signals
And if VCC2 to be connected to ground, should we ground it using a capacitor or can be directly connected to ground
Thanks and Regards
Abishek V