Post Go back to editing

no pixel clock output

Thread Summary

The user is troubleshooting an issue with the MAX96717/MAX96724 eval boards where the CKA clock is not running, despite valid data on the diff lanes and CKC clock. The final answer directs the user to Analog Devices' technical support pages for further assistance, without providing a specific solution. Configuration details include enabling the CSI output and setting the GMSL-A link and D-PHY lane mappings.
AI Generated Content
Category: Software
Product Number: max96724
Software Version: CSI config tool 1.6

I have an FPGA generated test pattern that I know works via connecting directly to an orin nano.

When I insert the MAX96717/MAX96724 eval boards in between and probe the diff lanes on the output of the MAX96724 I see valid data but I don't see any output clock. If I force all clocks to run (bit 7 on 0x8A0) then for some reason I see a clock on CKC but still nothing on CKA.

Is there some reason why CKA isn't running?

I'm using this output from the CSI configuration tool

//
// CSIConfigurationTool
//
// GMSL-A / Serializer: MAX96717 (Pixel Mode) / Mode: 1x4 / Device Address: 0x84 / Multiple-VC Case: Single VC / Pipe Sharing: Separate Pipes
// PipeZ:
// Input Stream: VC0 YUV422_8bit PortB (D-PHY)

// Deserializer: MAX96724 / Mode: 4 (1x2) / Device Address: 0x4E
// Pipe0:
// GMSL-A Input Stream: VC0 YUV422_8bit PortB - Output Stream: VC0 YUV422_8bit PortC (D-PHY)

0x04,0x4E,0x04,0x0B,0x00, // BACKTOP : BACKTOP12 | CSI_OUT_EN (CSI_OUT_EN): CSI output disabled
// Link Initialization for Deserializer
0x04,0x4E,0x00,0x06,0xF1, // DEV : REG6 | (Default) LINK_EN_A (LINK_EN_A): Enabled | LINK_EN_B (LINK_EN_B): Disabled | LINK_EN_C (LINK_EN_C): Disabled | LINK_EN_D (LINK_EN_D): Disabled
0x04,0x4E,0x00,0x03,0xFE, // DEV : REG3 | (Default) DIS_REM_CC_A (GMSL Link A I2C Port 0): Enabled | DIS_REM_CC_B (GMSL Link B I2C Port 0): Disabled | DIS_REM_CC_C (GMSL Link C I2C Port 0): Disabled | DIS_REM_CC_D (GMSL Link D I2C Port 0): Disabled
0x00,0x01, // Warning: The actual recommended delay is 5 usec.
// Video Transmit Configuration for Serializer(s)
0x04,0x84,0x00,0x02,0x03, // DEV : REG2 | VID_TX_EN_Z (VID_TX_EN_Z): Disabled
//
// INSTRUCTIONS FOR GMSL-A SERIALIZER MAX96717
//
// MIPI D-PHY Configuration
0x04,0x84,0x03,0x30,0x00, // MIPI_RX : MIPI_RX0 | (Default) RSVD (Port Configuration): 1x4
0x04,0x84,0x03,0x83,0x00, // MIPI_RX_EXT : EXT11 | Tun_Mode (Tunnel Mode): Disabled
0x04,0x84,0x03,0x31,0x10, // MIPI_RX : MIPI_RX1 | ctrl1_num_lanes (Port B - Lane Count): 2
0x04,0x84,0x03,0x32,0xE0, // MIPI_RX : MIPI_RX2 | (Default) phy1_lane_map (Lane Map - PHY1 D0): Lane 2 | (Default) phy1_lane_map (Lane Map - PHY1 D1): Lane 3
0x04,0x84,0x03,0x33,0x04, // MIPI_RX : MIPI_RX3 | (Default) phy2_lane_map (Lane Map - PHY2 D0): Lane 0 | (Default) phy2_lane_map (Lane Map - PHY2 D1): Lane 1
0x04,0x84,0x03,0x34,0x00, // MIPI_RX : MIPI_RX4 | (Default) phy1_pol_map (Polarity - PHY1 Lane 0): Normal | (Default) phy1_pol_map (Polarity - PHY1 Lane 1): Normal
0x04,0x84,0x03,0x35,0x00, // MIPI_RX : MIPI_RX5 | (Default) phy2_pol_map (Polarity - PHY2 Lane 0): Normal | (Default) phy2_pol_map (Polarity - PHY2 Lane 1): Normal | (Default) phy2_pol_map (Polarity - PHY2 Clock Lane): Normal
0x04,0x84,0x03,0x31,0x50, // MIPI_RX : MIPI_RX1 | ctrl1_deskewen (Controller 1 Deskewen): Enabled
// Controller to Pipe Mapping Configuration
0x04,0x84,0x03,0x08,0x64, // FRONTTOP : FRONTTOP_0 | (Default) RSVD (CLK_SELZ): Port B | (Default) START_PORTB (START_PORTB): Enabled
0x04,0x84,0x03,0x11,0x40, // FRONTTOP : FRONTTOP_9 | (Default) START_PORTBZ (START_PORTBZ): Start Video
0x04,0x84,0x03,0x18,0x5E, // FRONTTOP : FRONTTOP_16 | mem_dt1_selz (mem_dt1_selz): 0x5E
// Pipe Configuration
0x04,0x84,0x00,0x5B,0x00, // CFGV__VIDEO_Z : TX3 | TX_STR_SEL (TX_STR_SEL Pipe Z): 0x0
//
// INSTRUCTIONS FOR DESERIALIZER MAX96724
//
// Video Pipes And Routing Configuration
0x04,0x4E,0x00,0xF0,0x60, // VIDEO_PIPE_SEL : VIDEO_PIPE_SEL_0 | (Default) VIDEO_PIPE_SEL_0 (Pipe 0 GMSL2 PHY): A | VIDEO_PIPE_SEL_0 (Pipe 0 Input Pipe): X
0x04,0x4E,0x00,0xF4,0x01, // VIDEO_PIPE_SEL : VIDEO_PIPE_EN | (Default) VIDEO_PIPE_EN (Video Pipe 0): Enabled | VIDEO_PIPE_EN (Video Pipe 1): Disabled | VIDEO_PIPE_EN (Video Pipe 2): Disabled | VIDEO_PIPE_EN (Video Pipe 3): Disabled | STREAM_SEL_ALL (Stream Select All): Disabled
// Pipe to Controller Mapping Configuration
0x04,0x4E,0x09,0x0B,0x07, // MIPI_TX__0 : MIPI_TX11 | MAP_EN_L (MAP_EN_L Pipe 0): 0x7
0x04,0x4E,0x09,0x0C,0x00, // MIPI_TX__0 : MIPI_TX12 | (Default) MAP_EN_H (MAP_EN_H Pipe 0): 0x0
0x04,0x4E,0x09,0x0D,0x1E, // MIPI_TX__0 : MIPI_TX13 | MAP_SRC_0 (MAP_SRC_0 Pipe 0 DT): 0x1E | (Default) MAP_SRC_0 (MAP_SRC_0 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x0E,0x1E, // MIPI_TX__0 : MIPI_TX14 | MAP_DST_0 (MAP_DST_0 Pipe 0 DT): 0x1E | (Default) MAP_DST_0 (MAP_DST_0 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x0F,0x00, // MIPI_TX__0 : MIPI_TX15 | (Default) MAP_SRC_1 (MAP_SRC_1 Pipe 0 DT): 0x0 | (Default) MAP_SRC_1 (MAP_SRC_1 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x10,0x00, // MIPI_TX__0 : MIPI_TX16 | (Default) MAP_DST_1 (MAP_DST_1 Pipe 0 DT): 0x0 | (Default) MAP_DST_1 (MAP_DST_1 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x11,0x01, // MIPI_TX__0 : MIPI_TX17 | MAP_SRC_2 (MAP_SRC_2 Pipe 0 DT): 0x1 | (Default) MAP_SRC_2 (MAP_SRC_2 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x12,0x01, // MIPI_TX__0 : MIPI_TX18 | MAP_DST_2 (MAP_DST_2 Pipe 0 DT): 0x1 | (Default) MAP_DST_2 (MAP_DST_2 Pipe 0 VC): 0x0
0x04,0x4E,0x09,0x2D,0x00, // MIPI_TX__0 : MIPI_TX45 | (Default) MAP_DPHY_DEST_0 (MAP_DPHY_DST_0 Pipe 0): 0x0 | (Default) MAP_DPHY_DEST_1 (MAP_DPHY_DST_1 Pipe 0): 0x0 | (Default) MAP_DPHY_DEST_2 (MAP_DPHY_DST_2 Pipe 0): 0x0
// MIPI D-PHY Configuration
0x04,0x4E,0x08,0xA0,0x01, // MIPI_PHY : MIPI_PHY0 | phy_4x2 (Port Configuration): 4 (1x2)
0x04,0x4E,0x09,0x0A,0x50, // MIPI_TX__0 : MIPI_TX10 | CSI2_LANE_CNT (Port C - Lane Count): 2
0x04,0x4E,0x08,0xA3,0xE4, // MIPI_PHY : MIPI_PHY3 | (Default) phy0_lane_map (Lane Map - PHY0 D0): Lane 0 | (Default) phy0_lane_map (Lane Map - PHY0 D1): Lane 1
0x04,0x4E,0x08,0xA5,0x00, // MIPI_PHY : MIPI_PHY5 | (Default) phy0_pol_map (Polarity - PHY0 Lane 0): Normal | (Default) phy0_pol_map (Polarity - PHY0 Lane 1): Normal | (Default) phy0_pol_map (Polarity - PHY0 Clock Lane): Normal
0x04,0x4E,0x09,0x03,0x81, // MIPI_TX__0 : MIPI_TX3 | (Default) DESKEW_INIT (Controller 0 Auto Initial Deskew): Enabled | DESKEW_INIT (Controller 0 Initial Deskew Width): 2 * (32K) UI
0x04,0x4E,0x09,0x04,0x81, // MIPI_TX__0 : MIPI_TX4 | (Default) DESKEW_PER (Controller 0 Periodic Deskew): Enabled | (Default) DESKEW_PER (Controller 0 Periodic Deskew Width): 2 * (1K) UI
0x04,0x4E,0x1C,0x00,0xF4, // (config_soft_rst_n - PHY0): 0x0
// This is to set predefined (coarse) CSI output frequency
// CSI Phy 0 is 800 Mbps/lane.
0x04,0x4E,0x1C,0x00,0xF4, // (Default)
0x04,0x4E,0x04,0x15,0x28,
0x04,0x4E,0x1C,0x00,0xF5, // | (Default) (config_soft_rst_n - PHY0): 0x1
0x04,0x4E,0x08,0xA2,0x14, // MIPI_PHY : MIPI_PHY2 | phy_Stdby_n (phy_Stdby_1): Put PHY1 in standby mode | phy_Stdby_n (phy_Stdby_2): Put PHY2 in standby mode | phy_Stdby_n (phy_Stdby_3): Put PHY3 in standby mode
0x04,0x4E,0x04,0x0B,0x02, // BACKTOP : BACKTOP12 | CSI_OUT_EN (CSI_OUT_EN): CSI output enabled
// Video Transmit Configuration for Serializer(s)
0x04,0x84,0x00,0x02,0x43, // DEV : REG2 | VID_TX_EN_Z (VID_TX_EN_Z): Enabled

Parents Reply Children
No Data