Post Go back to editing

Digital Isolators and IsoPower Operation at High Altitude

Category: Hardware
Product Number: ADM2565EBRNZ, ADM2565E

I would like to use these devices in an application that can go to 55,000 feet in altitude.

I have designed in a bunch of Digital Isolators with and without power.

ADM2565EBRNZ

ADUM342E0BRQZ

ADUM3151BRSZ

ADUM3152BRSZ

ADUM6202CRWZ

 

I understand clearance and creepage across the package and between pins etc (and on the PCB itself) and the need to derate at higher altitudes. Also, how conformal coating etc can help mitigate.

What I am not sure about is the possible affects, if any, on the breakdown of the device internal transformers / isolation barrier?

Are they similar to transformers with an air gap, where the reduced dielectric at altitude can effect their performance significantly?

Will these devices even functionally operate (never mind the isolation) at 55,000 feet? 

Thanks

  • Hi, 

    There are planar transformers inside these products. The bottom coil of the coil is top layer metal on the die. The bottom coil is overcoated with multiple layers of polyimide and then the top coil is layed down on the polyimide. The package is then transfer molded around that die assembly. It is a cemented joint so I would expect the limitation to be the package and the effects of Paschen's law.

    There are standard isolators in ceramic packages with radiation hardened die variants like ADuM141ES and ADuM7442S that are intended to LEO apps. The working voltage is rather limited compared to industrial market parts though. 

    Regards,

    Jason

      

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.