Post Go back to editing

max31732

Thread Summary

The user inquires about the MAX31732 IC's comparator mode, specifically if there is a register to adjust the de-assert temperature threshold beyond the default 2°C. The final answer directs the user to visit the Analog Devices technical support pages for further assistance, without providing a specific register or configuration detail.
AI Generated Content
Category: Hardware
Product Number: MAX31732, MAX3173

Hi all,

In my design I want to use MAX31732 IC for temperature sensing. As per my understanding, in comparator mode alarm signals asserted after reaching programmable threshold value and de-asserts alarm signals after reduction in 2Deg C from programmed value, is there any register to increase the de-assert the temperature threshold value after which we want to de-asset the alarm signals?

Edit Notes

add legacy maxim product tag
[edited by: AAlessandro at 6:41 AM (GMT -4) on 4 Oct 2024]