Hi,
I had made a design with LTM2881MPY-3 transceivers. There was a overcurrent failure on the 5V line of on my PCB.
In my design 5V was used as VCC of LTM2881 IC. After the overcurrent failure I'm trying to find the root cause and what ICs have been affected by the failure.
I checked the impedance from B6, B7 and B8 pins to GND pins (B1 to B5) and I'm observing the following:
VCC Pin GND pin Impedance (in ohms)
B6, B7 & B8 B3,B4 & B5 1.19 kohms
B6, B7 & B8 B2 18.15 kohms
B6, B7 & B8 B1 45.7 kohms
I wanted a know if these readings are alright or has the IC been damaged.
Thank you,
Abhishek