Post Go back to editing

ADM3050E behaviour when unpowered

Category: Datasheet/Specs
Product Number: ADM3050E

Can you confirm that if an unpowered ADM3050E node is on a CAN bus, then the prescence of this unpowered node will not impede the bus. 

Is there a brownout feature such that if its power droops it will cut itself off the bus?

Example: 

CAN-FD bus with 5 nodes, operating at 5 Mbps

Node 2 uses an ADM3050E, and is powered down but remains connected to the bus. 

Will nodes 1,3,4,5 still be able to communicate on the CAN bus?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.