Hello,
We are evaluating the MAX14189A (the EV kit) to be the physical controller of our io-link stack.
We are trying to test the establish-communication sequencer (auto detect) but for some reason it is failing. We are
using the io-link device transceiver utility to read and write to registers directly (without using our stack) just for this test.
The WURQInt is generated but the sequencer is failing to detect the correct COM baud rate. Same thing happens with or without the sensor.
We are testing with PV7003 & IF6124 , both from IFM, but both are not detected.
So is there an Application Note that can help? , if not, what should be the register settings for this test?
We are using the default HW configuration of the EV kit.