Post Go back to editing

Need to know the difference Marking on the same divices.

Category: Datasheet/Specs
Product Number: MAX3161EEAG+T, MAX3161E

Good day.

As I wrote on the title, I wonder the difference marking between MAX3161EEAG and MAX3161EEG and any differences they have.

Are they different due to the site of manufacturing? 

Or is it related to your M&A with Maxim Integrated?

Thank you.

Best regards,

Parents
  • Thank you for your question.

    The MAX3161 and MAX3161E are different devices.  They are very similar, but there are some differences, for example the MAX3161E has a lower VCC shutdown current, some slightly reduced leakage currents, and a higher ESD (on R_IN, T_OUT, A, B, Y, and Z pins) than the MAX3161.

    The MAX3161EEAG is the MAX3161E device in a 24 TSSOP package with a -40degC to +85degC operating temperature range.

    Analog Devices does not make or sell a MAX3161EEG device. It is not documented online or anywhere in the datasheet. Do you have a purchase order from ADI or an authorized distributor for these parts?

    Thank you,

    Shasta

Reply
  • Thank you for your question.

    The MAX3161 and MAX3161E are different devices.  They are very similar, but there are some differences, for example the MAX3161E has a lower VCC shutdown current, some slightly reduced leakage currents, and a higher ESD (on R_IN, T_OUT, A, B, Y, and Z pins) than the MAX3161.

    The MAX3161EEAG is the MAX3161E device in a 24 TSSOP package with a -40degC to +85degC operating temperature range.

    Analog Devices does not make or sell a MAX3161EEG device. It is not documented online or anywhere in the datasheet. Do you have a purchase order from ADI or an authorized distributor for these parts?

    Thank you,

    Shasta

Children
No Data