I am trying to check my configuration for the LTM2889. I have it set so that the ON pin is set to 1 while S and RE are set to 0. I have a TXD line going into the LTM2889, but no RXD (using an internal loopback for now in the microcontroller).
There is no output CAN High or CAN Low signal being outputted from the LTM2889 that I can see on the oscilloscope, even though I can see the TXD line going into the LTM2889 is sending CAN messages. I do have an IXXAT USB-to-CAN on the other end of the CAN High and CAN Low lines that is not detecting any CAN messages received.
Is my configuration correct, or is there anything else I need to make sure of?