MAX22208
Recommended for New Designs
The MAX22208 provides four individually controllable 65V, 3.8AMAX half H-bridge drivers. It can be used to drive four solenoids, two brushed DC motors...
Datasheet
MAX22208 on Analog.com
Is it possible to obtain a pspice model of this part?
We do not have a Spice model for the MAX22208 but we do have a LTSpice model for the MAX22205 MAX22205 Datasheet and Product Info | Analog Devices
Hi,
Can the LTSpice model be converted into PSPICE ? I have tested a little in the LTSpice environment with the MAX22205, but it is very limited and cumbersome what I can do there. It would help a lot if I could get a pspice model of both.
LTSpice is a free download tool from ADI and we provide models for this format. ADI does not have a PSPICE model for this chip.