ADM2863E
Recommended for New Designs
The ADM2861E, ADM2863E, ADM2865E, and ADM2867E are 5.7 kV rms signal and power isolated RS-485 transceivers. These devices are designed for balanced transmission...
Datasheet
ADM2863E on Analog.com
Hello,
I am working on an design using the ADM2863. I connected it according to the datasheet and its working fine so far. Only thing that's not as I expected is the power consumption of the IC. I'm not sure if it's a mistake on my side or if it is normal that my board uses ~ 30mA more (12V > LDO > 3V3 > ADM2863) all the time as soon as the ADM2863 is on it. This happens as soon as I power the board (not executing code), if its sending a message every second and doesn't change if I set TX/RX enable signals high or low (It only stops working, as expected). Its the 3rd identical board I have tested and I checked my circuit multiple times. So I'm wondering if that's normal for this device or if I am missing something here. Is there a way to "turn it off" or "let it sleep" if unused?
Without the components on V_isoout / V_isoin its not working (obviously) but also only increasing the consumption ~5mA.

R17&18 are not in place and R19 makes no difference.
In previous designs I measured the consumption of the ADM2582 and it was using ~6mA on an DC/DC so I was expecting this one to need less current. Especially as the max. power ratings in the Datasheet of this newer IC are lower than the ones in the ADM2582 datasheet.
Thanks
Hi Fizzl,
These current levels are normal and with expected levels for this part. See page 4 of the datasheet, where the expected Vcc supply current with the bus unloaded can range from a typical of 20mA up to 53mA, so your ~30mA is right in the range.
The ADM2582 uses a different isolated power supply circuit which is more efficient, but it is also a stronger source of common-mode emissions and so requires a careful PCB layout with multiple layers to form stitching capacitor to control these emissions. The ADM2863's power supply circuit is greatly improved from the power supply's common-mode emissions perspective, but this improvement comes at the cost of a greater supply current.
Unfortunately this part doesn't natively offer a lower power standby option. If your application is able to tolerate the approximately 10ms start up time for the power supply, you could add a switch/pass transistor to switch the Vcc supply on and off. It is OK to leave VIO powered and if DE and TxD are both low, the supply current will be less than 1mA. If you implement this mode, I'd suggest also making sure that nRE is pulled high so that RxD is put into a high-Z state.
Eric
Hi Eric,
thank you for your detailed answer. I was pretty much expecting this after all my tests and, as you said, as the datasheet already mentions this. But as the ADM2582s datasheet states >100mA in some scenarios I wanted do be sure that i haven't missed anything here.
Good to know that I can turn it off that way. I'll try that and see what the consumption is after that - additional 10ms are no problem here.
As an alternative, is there a low-power isolated 485 IC that would fit (ideally) this footprint and maybe even as a drop in replacement?
Thanks
Fizzl