Post Go back to editing

High side MOSFET driver

Category: Hardware
Product Number: ADuM4135

I want to use ADuM4135 in my PCB. In my design I have a high voltage pulse generator which can output up to 2KV pulses (up to 2MHz). I want to connect/short the output of this generator with different electrical points. I am using series of MOSFET for my case. MOSFET will turn on before generator and stays on until generator stop output pulses. For driving MOSFETs I want to use ADuM4135 ICs (a single PCB may require over 40 ICs). 
Now, my question is, can I use ADuM4135 for my case, if yes, can you please provide some reference files.

Thanks.

Parents Reply
  • The example provided in the Ltspice is for low side MOSFET driver and also there is no explanation. Please, check the .asc file which I provided. I want to use ADuM4146A as a high side MOSFET driver. What I want is, where should I connect my MOSFET source pin? 
    Before going to PCB design I want to confirm the output in simulation. I upload the file from the example folder of Ltspice, can you update it for high side MOSFET driver, I tried but the result is different. 
    ADuM4146A.asc

Children
No Data