Post Go back to editing

MAX4995C

Category: Datasheet/Specs
Product Number: MAX4995C

I would like to use the MAX4995C part with a lower current limit than spec'd in the datasheet. The normalized current limit accuracy is only spec'd across the 50mA to 600mA range. I would like to use this part with a current limit of around 5mA. I assume the accuracy is no longer guaranteed, but how far off? Are there any other parameters I should be concerned with at such a low current limit? Please provide any recommendations, much appreciated! 



Legacy Maxim Product
[edited by: AAlessandro at 6:38 AM (GMT -4) on 18 Jul 2024]