Hi,
We have design where we require SPI Isolation between the SOM and DAC (AD5781).
We want to run the SPI at max allowable CLK freq of 35MHz.
One of the SPI Isolator we shortlisted is MAX14483.
According to the datasheet and link below, it can support upto 100MHz clock.
Digital Signal Isolation for a Better Design
But in the app note below, the max allowable SPI clk freq calculation suggests different value and limitations.
https://www.analog.com/en/resources/app-notes/an-1478.html
I am not sure if I am confusing something here or understanding is wrong.
So, please can you confirm if the P/N MAX14483 can be used at spi clk freq of 35-40MHz reliably.
Thanks & Regards,