Post Go back to editing

ADM2795E in RS422 mode, DO0160G protection

Thread Summary

The user asked if large external resistors are necessary for an ADM2793E-EP receiver on an RS422 bus when testing for DO-160G level 4 transients. The final answer confirms that the resistors are required for both transmitters and receivers to protect against transients. The user was referring to the 33 or 47 Ohm resistors mentioned in the ADM2795E-EP datasheet and Application Note 1468.
AI Generated Content
Category: Hardware
Product Number: ADM2795E

Hopefully a simple question. If we are using the ADM2793E-EP in an application on an RS422 bus and it is a receiver only, do we need the large, external resistors, if testing to DO-160G level 4 transients?

Parents Reply Children
No Data