Post Go back to editing

V-by-One HS Isolation with ADN4624

Thread Summary

The user encountered issues with V-by-One HS signal isolation using the EVAL-ADN4624EB1Z between THCV241A and THCV242A boards. The problem was due to incorrect silkscreen labeling on the EVAL board, causing the DIN+ and DIN- signals to be connected incorrectly. The solution involved swapping the DOUT+ and DOUT- connections to match the correct polarity, as the ADN4624 does not invert the logic. The eye diagrams were confirmed to be good, and the CDR in the receiver was locking, indicating proper signal integrity.
AI Generated Content
Category: Hardware
Product Number: ADN4624

Hello

I would like to isolate the V-by-One HS signal with ADN4624.
I bought EVAL-ADN4624EB1Z and put it between the board of the V-by-One HS transmitter (THCV241A) board and the board of the V-by-One HS receiver (THCV242A) board as the attached block diagram.

Block Diagram

The image streaming fails but the part of the signal seems to be isolated and transferred by ADN4624 because the CDR in the receiver in LOCK.
However, the receiver detects the error in the V-by-One HS data stream.

It would be appreciated if you review this post and give me advise of the debug.

I can see the streaming image if the transmitter board and receiver board connect via the coax cable without EVAL-ADN4624EB1Z.
There is no error asserted in the V-by-One HS receiver.
Thus, the transmitter and receiver settings and boards are fine.

I shorted the non-use DIN+ signals with 1.8V and the non-use DIN- signals with GND.
The VDD1 and VDD2 of ADN4624 are 1.8V on the EVAL-ADN4624EB1Z.

I scoped the input V-by-One HS waveform at the 100ohm termination resistor at ADN4624 input.

ADN4624 DIN+/- input


Could you review the waveform and give me some advise?

Best regards,

Larry

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.