Post Go back to editing

ADUM1410

Category: Hardware
Product Number: ADUM1410

Hello.

I'm using ADuM1410 and have a question for Pin#10:CTRL2.

Accoring to data sheet, "Default Output Control. Controls the logic state the outputs assume when the input power is off. VOA, VOB, VOC, and VOD outputs are high when CTRL2 is high or disconnected and VDD1 is off. VOA, VOB, VOC, and VOD outputs are low when CTRL2 is low and VDD1 is off. When VDD1 power is on, this pin has no effect." What voltage is threshold of VDD1 power on/off in case VDD1 5V.