The MAX22192_EVKITB in daisy chain mode is having issues: the U2 slave is not responding, and the U1 slave is providing pin input status but is unresponsive to write commands.


For communication iam using an STM microcontroller which is running SPI at 5Mhz

Made connections as per above and left out 7,8,9,10 pin connections, tried in indipedant slave and it is working.For power supply board is being supplied by 24v for field side and 3V3 for logic side.
First packet iam sending write to led matrix register for u1 and for u2 writing 0 in the fault1 register.
I have been sitting on this for a while now, as i need to calculation the propagation delay with our work enviornment. any help would be apreciated.
Edit Notes
Updated subject[edited by: Sarun at 10:58 AM (GMT -4) on 20 Jun 2024]