Post Go back to editing

MAX3160E FAST-MODE pin termination

Category: Datasheet/Specs
Product Number: MAX3160E

The MAX3160E FAST-MODE operation describes the pin as asserted or unasserted.  In this context is unasserted the same as GND / De-assertion?  I am reviewing schematics where they left this pin floating and I want to confirm the terminology unasserted doesn't mean floating here.  I see no mention of internal pull-up/down termination on this pin.  I am assuming this pin needs to be pulled to ground or VCC.  

Parents
  • Hello,

    Thank you for your question!

    You are correct - FAST is asserted when connected high (> 2.4V) and unasserted when connected low (<0.8V).  So, yes, it would be considered as unasserted when connected to ground.

    There is no internal pull-up or pull-down on the FAST pin. You are correct that the pin needs to be connected high (VCC) or low (GND) to enable/disable fast mode.

    Best,

    Shasta

Reply
  • Hello,

    Thank you for your question!

    You are correct - FAST is asserted when connected high (> 2.4V) and unasserted when connected low (<0.8V).  So, yes, it would be considered as unasserted when connected to ground.

    There is no internal pull-up or pull-down on the FAST pin. You are correct that the pin needs to be connected high (VCC) or low (GND) to enable/disable fast mode.

    Best,

    Shasta

Children
No Data