Post Go back to editing

MAX3160E FAST-MODE pin termination

Thread Summary

The user asked if 'unasserted' for the FAST pin on the MAX3160E means floating. The engineer confirmed that 'unasserted' means the pin is connected to ground (GND), and 'asserted' means it is connected to VCC. The FAST pin has no internal pull-up or pull-down and must be explicitly connected to enable or disable fast mode.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX3160E

The MAX3160E FAST-MODE operation describes the pin as asserted or unasserted.  In this context is unasserted the same as GND / De-assertion?  I am reviewing schematics where they left this pin floating and I want to confirm the terminology unasserted doesn't mean floating here.  I see no mention of internal pull-up/down termination on this pin.  I am assuming this pin needs to be pulled to ground or VCC.  

  • Quoted portion of datasheet

    "Fast-Mode Operation The FAST control input is used to select the slew-rate limiting of the RS-232 transmitters and the RS-485/ RS-422 drivers. With FAST unasserted, the RS-232 transmitters and the RS-485/RS-422 driver are slew-rate limited to reduce EMI. RS-232 data rates up to 1Mbps and RS-485/RS-422 data rates up to 10Mbps are possible when FAST is asserted. FAST can be changed during operation without interrupting data communications."

  • Hello,

    Thank you for your question!

    You are correct - FAST is asserted when connected high (> 2.4V) and unasserted when connected low (<0.8V).  So, yes, it would be considered as unasserted when connected to ground.

    There is no internal pull-up or pull-down on the FAST pin. You are correct that the pin needs to be connected high (VCC) or low (GND) to enable/disable fast mode.

    Best,

    Shasta

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.