Post Go back to editing

When transmitter is disabled, on LT1785, there is current source pulling the -DATA pin to VCC through a 100Ω resistor to ground. I replaced the 1785 with a ST4E1240DT and the 100Ω pulled the -DATA pin to ~300mV. Changing back to the 1785 my problem ret

Category: Hardware
Product Number: LT1785

When transmitter is disabled, on LT1785, there is current source pulling the -DATA pin to VCC through a 100Ω resistor to ground. I replaced the 1785 with a ST4E1240DT and the 100Ω pulled the     -DATA pin to ~300mV. Changing back to the 1785 my problem returned.  What should I expect the leakage current to be? Cause right now it appears to be around 50mA.

Here is the transmission of 0x03. 1st 3 bits shown,

Bottom trace is Tx enable, top is -D.

In my application I have 100Ω pull up on +D and on -D.

I invert TX data from UART as the enable.

The 100Ω resistor was suppose to keep -D low until enable occurs.

Parents Reply
  • Terry - I tested a LTC1785 on a EVAL-RS485HDEBZ eval board, VCC = 5V, /RE = 5V, DI = 0V, and drive DE with a 1khz square wave, with 100 ohm pull up and pull down resistors to replicate your circuit. The part performed as expected with AB unloaded and with a 120ohm load across AB. Scope shot has CH1 = DI, CH2 = A and CH3 = B. I think the device you have is faulty - have you ordered a free samples from ADI and tested those ?

Children