Post Go back to editing

When transmitter is disabled, on LT1785, there is current source pulling the -DATA pin to VCC through a 100Ω resistor to ground. I replaced the 1785 with a ST4E1240DT and the 100Ω pulled the -DATA pin to ~300mV. Changing back to the 1785 my problem ret

Category: Hardware
Product Number: LT1785

When transmitter is disabled, on LT1785, there is current source pulling the -DATA pin to VCC through a 100Ω resistor to ground. I replaced the 1785 with a ST4E1240DT and the 100Ω pulled the     -DATA pin to ~300mV. Changing back to the 1785 my problem returned.  What should I expect the leakage current to be? Cause right now it appears to be around 50mA.

Here is the transmission of 0x03. 1st 3 bits shown,

Bottom trace is Tx enable, top is -D.

In my application I have 100Ω pull up on +D and on -D.

I invert TX data from UART as the enable.

The 100Ω resistor was suppose to keep -D low until enable occurs.

Parents Reply
  • Yes, you are correct. U4 pin 6 is "A" or "+D" and U4 pin 7 is "B" or "-D". I isolated the MAX211 by removing pins connected to U 4 pins 6 &7. U4 pin 6 is acting as I expect.

    U4 pin 7 is not. I expect pin 7 to be low when "TE" is low (U4 pin3).

    In the photo below, Yellow is "TE", U4 pin 3.

    Blue is "A", U4 pin 6. (Pulled up to VCC thru 100Ω) looks correct

    Pink is "B", U4 pin 7. (Pulled down to GND thru 100Ω) should a square wave.

    And again, a ST4E1240DT works as expected.

Children