Hello.
I have questions about MAX232A.
Is the variation of the internal resistance of the MAX232A receiver from a minimum of 3 kΩ to a maximum of 7 kΩ?
Also, does the minimum 3kΩ to maximum 7kΩ vary from device to device?
Best regard,
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX232A
Production
The MAX220–MAX249 family of line drivers/receivers is intended for all EIA/TIA-232E and V.28/V.24 communications interfaces, particularly applications...
Datasheet
MAX232A on Analog.com
Hello.
I have questions about MAX232A.
Is the variation of the internal resistance of the MAX232A receiver from a minimum of 3 kΩ to a maximum of 7 kΩ?
Also, does the minimum 3kΩ to maximum 7kΩ vary from device to device?
Best regard,
Hello,
Yes, the MAX232A also has a 3kohm to 7kohm receiver input impedance to ground. The 3kohm to 7kohm does not vary from device to device - it is standard across all devices in this family.
Thank you,
Shasta
Hi, ShastaThomas
Thanks for the reply.
I have one more question.
Do you mean that the internal termination resistance varies from 3kΩ to 7kΩ, depending on the conditions of use, rather than varying from device to device?
Best regards.
Hi,
The internal termination will have some process variation (device to device) and likely has some temperature dependence. Since there are no TOCs of the receiver, I can't speak to exactly how much variation might occur but I am guessing it would not be much. It is important to note that the internal termination is guaranteed to be within the stated range (3kohm to 7kohm) for every device and over the entire supply and temperature operating ranges, so it should never fall outside of those limits under normal operating conditions.
Thank you,
Shasta