Post Go back to editing

Driver design for SiC MOSFET Full Bridge Inverter with Vds=100V, can not go higher than Vds=50V (SiC MOSFET rated for 650V)

Thread Summary

The user encountered high peak currents and oscillations in a full-bridge inverter using ADUM4121 isolated gate drivers and C3M0120065K SiC MOSFETs at 40V DC link voltage. Increasing the gate resistance to 50 Ohms resolved the issue, but the user is seeking a more optimal solution. Oscilloscope images of the double pulse test showed strong oscillations during turn-on and turn-off, suggesting possible issues with the gate driver or parasitic capacitances. The user is open to further discussion and assistance.
AI Generated Content
Category: Hardware
Product Number: adum4121

Hello everyone,

I am writing to you in search of help. I've spent a couple of weeks trying to figure out what I'm doing wrong, but I'm still not clear on what I'm doing.

I am working on the design and prototype of a full-bridge inverter and have chosen ADUM4121 as the isolated gate driver and C3M0120065K as the SiC MOSFET (Vds=650V, Id=22A) for the converter. Both manufacturers (Wolfspeed and Analod Devices) recommend them as a matching pair.

Each SiC MOSFET has its driver and unregulated isolated DC-DC source (R15P21503D). Therefore no boot trap is required.

The inverter's DC link is rated at 100V, and the load is a series RL (R=10 Ohms and L=4mH).

The modulation is a unipolar sinusoidal PWM.

I've followed the design of KIT-CRD-8FF65P (650V), which uses the same driver and isolated DC source I use. However, for the new SiC MOSFET, I changed the gate resistor to Rg(on)=10 Ohm and Rg(off)=5 Ohm (Cgs and Rgs are avoided).

The problem is that although the taken example is made for Vds=650V and my design is made for Vdc=100V, when I reach 40V from the DC source (DC link) some high peak currents start to appear at the SiC MOSFET drain (4 times higher than the nominal current), killing my SiC MOSFET devices.

The only solution that worked was to increase the Rg(on,off) from 10 ohms to 50 Ohms, which is too high for a common application.

Simulations work perfectly, but the prototype does not.

Is there something I've missed?
Is 50 ohm too high as gate resistance Rg?
The schematic is attached, and I can attach oscilloscope screens if needed.

Thank you very much for your support!

  • Hi PabloGuicharrousse,

    How much dead time are you applying on the PWM signals? Did you try to increase the dead time to rule-out possible shoot through issues?

    An oscilloscope capture of the over current event and PWM signals can help to debug the issue.

    Regards,
    Luca
      

  • Hello Luca,

    Thanks for your reply!

    I increased the dead time (400ns with 20kHz carrier frequency for the PWM), but the circuit has the same limitation.

    As soon as I get the oscilloscope images, I'll be back.

    Kind regards,

    Pablo

  • Hi Luca,

    I'm back on my Full-Bridge Inverter, and for more accuracy regarding my problem, I have taken screenshots for the Double Pulse Test. Vdd=70[V].


    Considering the previous circuit:

    • Device Under Test is the U2
    • U1 is permanently off.
    • U3 is permanently on.
    • U4 is permanently off.

    Some strong oscillations appear during the turn-on and turn-off drain current.

    The turn-on ID current does not even show clear behaviour.

    I am trying to find some ideas on how to suppress them. I think that it could be related to capacitors C16 and C15, but not sure.

    Do you have any idea on what could cause that oscilations when using ADUM4121?

    Thanks for your help!

    Double Pulse Test (yellow Vds, blue Id)

    Turn-on (yellow Vds, blue Id)

    Turn-off (yellow Vds, blue Id)

    Kind regards,

    Pablo

  • SOLVED!

    If anyone is struggling with a similar issue, please do not hesitate to contact me.

    Kind regards,

    Pablo Guicharrousse

  • Hi Pablo, I too facing the same problem in the gate driver, and have oscillation at turn-off interval (but starts after delay. How do you resolve the problem.

  • Hi Ak86,

    There were no problem with the schematic, connections, values or drivers.

    The problem was the kind of probes I used to meassure current and voltage.

    In the case of current, I was using normal current clamp probes (Fluke i30s AC/DC Current Clamp), wich have a reduced bandwidth to meassure  fast transients. I recomend to use Rogowsky Coils (really helpfull for fast transientents).

    In the case of voltage, the differential probes I used had a restricted ratio. Therefore, when I crossed the maximum voltage limit, the isolation of the voltage probes failed and made a loop to the ground.

    In summary, everything was in my case related to the instrument I used to meassure voltage and current. So, try to use Rogowsky coils for transient current, and check that the limits of the differential voltage probes match your ratings.

    In addition, some of that oscillation come from parasitic inductances, wich need to be solved by desing.

    I hope this answer helps you.

    Best regards,