Post Go back to editing

About LTC4331 Address Settings

Thread Summary

Q1: It is acceptable to set only the Local address and disable the Remote side on the LTC4331, as the Remote side's internal I2C device is automatically disabled. Q2: For the Remote configuration, the A1/A2 pins are irrelevant and can be set to any value, but must respect the ABSMAX limitations.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC4331

About LTC4331 Address Settings
Q1: Is it okay to set only the Local address and disable the Remote side?
Q2: If address specification is required for Remote as well, do terminal settings A1 and A2 need to be the same value for Local and Remote?

Parents
  • Hi Uboti,

    Q1: yes.  Note that this is how the part behaves since remote side part automatically disables that part's internal I2C device regardless of the address pin settings.  For the LTC4331 serial extender, there can only be one functioning internal I2C device in the link and it is located at the local side (assuming that its enabled via its address pins).

    Q2: When the LTC4331 part is configured to be in the remote configuration, it disables its internal I2C device and ignores the address setting pins A1/A2.  Therefore, the connections/configuration for these pins is irrelevant (however, they still need to respect the ABSMAX limitations on the pins).

    Eric

Reply
  • Hi Uboti,

    Q1: yes.  Note that this is how the part behaves since remote side part automatically disables that part's internal I2C device regardless of the address pin settings.  For the LTC4331 serial extender, there can only be one functioning internal I2C device in the link and it is located at the local side (assuming that its enabled via its address pins).

    Q2: When the LTC4331 part is configured to be in the remote configuration, it disables its internal I2C device and ignores the address setting pins A1/A2.  Therefore, the connections/configuration for these pins is irrelevant (however, they still need to respect the ABSMAX limitations on the pins).

    Eric

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.