Post Go back to editing

Typical input impedance/current

Category: Datasheet/Specs
Product Number: ADG3123

Hi

I have read the datasheet a couple of times and I can't seem to find a value for the input impedance or typical input current for a low or high signal. I'm developping a product with a sensor that has a maximum output current of 100 µA @ 5V and I want to interface the sensor to a PLC input. Will this work? The output voltages are 0V and 24V for the low and high value for the PLC. The outputs should be able to provide 15mA.

Hoping for a positive answer,

Kind regards

Karel