Post Go back to editing

ADN4624 with MC20901

Thread Summary

The user inquires about using a Meticom 20901 bridge IC to convert MIPI CSI-2 signals to LVDS for isolation with the ADN4624. The final answer confirms that this approach is feasible, but the user should verify with the Meticom manufacturer. The ADN4624 can handle the specified data rates and input voltages, but the compatibility of HS and LP signals across the isolation boundary remains to be confirmed.
AI Generated Content
Category: Hardware
Product Number: ADN4624

Hi ADI team,

I've been doing a bit of reading around trying to pass MIPI CSI-2 signals across an isolation boundary and it appears as though the most common approach is to use some form of FPGA to convert the signals into LVDS and then send these signals back to another FPGA on the other side.

What I'd like to know is whether using a dedicated MIPI D-PHY to LVDS bridge, for example the Meticom 20901, would eliminate the need for an FPGA on the "isolated" side. My thinking is as follows:

DESERIALISER (MIPI D-PHY / CSI-2 OUTPUT) -> METICOM 20901 (LVDS / CMOS OUTPUT) -> ADN4624 -> FPGA (LVDS / CMOS INPUT)

The proposed MIPI D-PHY output would be running at a channel rate of 800Mbps. Both the Meticom and the ADN4624 are capable of these data rates.

However, the HS and LP output voltages of the Meticom are 1.09 - 1.31V and 2.3 - 2.7V respectively. If I power both sides of the ADN4624 with a VDD = 1.8V as specified in the datasheet, the input side should be fine to accept incoming signals (as specified in the datasheet) but what becomes unclear is whether this is even feasible. Will the ADN4624 be able to correctly transmit both HS and LP signals across the isolation boundary without significant signal distortion? Or will it not work for another reason?

Any help you could offer would be greatly appreciated.

Many thanks,

Connor

Parents
  • Hi Connor,

    I'm facing the same problem you described here. Any chance you managed to make this work?

    I'm using he meticom chips to split the MIPI signal into HS and LP but I'm unsure the LP signals are compatible with ADN4624. If you found a solution to this, could you share more about it please?

    Thanks

    Simone

Reply
  • Hi Connor,

    I'm facing the same problem you described here. Any chance you managed to make this work?

    I'm using he meticom chips to split the MIPI signal into HS and LP but I'm unsure the LP signals are compatible with ADN4624. If you found a solution to this, could you share more about it please?

    Thanks

    Simone

Children
No Data