The reliability data on your site is not showing for MAX22196. SO please help me to get Reliability data.
thank you
MAX22196
Recommended for New Designs
The MAX22196 is an industrial octal digital input that translates eight industrial 24V or TTL level inputs to logic level outputs. The device has a serial...
Datasheet
MAX22196 on Analog.com
The reliability data on your site is not showing for MAX22196. SO please help me to get Reliability data.
thank you
Hi,
Here are the FIT rate data for the MAX22196 from 2016 to 2023.
- 0.02 FITs with 60% confidence level at 25°C
- 0.2 FITs with 60% confidence level at 55°C
Thanks,
Wei