The reliability data on your site is not showing for MAX22192 SO Please help me to get Reliability data.
thank you
MAX22192
Last Time Buy
The MAX22192 is an IEC 61131-2 compliant industrial
digital input device with integrated digital isolation. The
MAX22192 translates eight, 24V current...
Datasheet
MAX22192 on Analog.com
The reliability data on your site is not showing for MAX22192 SO Please help me to get Reliability data.
thank you
Hi,
Here are the FIT rate data for the MAX22192 from 2016 to 2023.
- 0.02 FITs with 60% confidence level at 25°C
- 0.2 FITs with 60% confidence level at 55°C
Thanks,
Wei